CLRC663ARD board and CLRC663PcSerial.3.6 test program

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLRC663ARD board and CLRC663PcSerial.3.6 test program

2,239件の閲覧回数
AlexBush
Contributor I

Hi everyone,

I am currently developing a wireless rfid identification node via CLRC663ARD.

The interface of CLRC663ARD configured to uart connection.
CLRC663ARD connected to PC via usb-uart converter.

I tested the operation of the CLEV663ARD using the CLRC663PcSerial.3.6 test program.

And CLRC663PcSerial.3.6 freezes when executing any jcf script from the program.

The freeze looks like this: commands from the script are successfully executed one by one. And one command does not receive a response from the board, after which the command is repeated again. And so on indefinitely.

I have tested all the scripts from the CLRC663PcSerial.3.6.

Is this normal?

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,165件の閲覧回数
AlexBush
Contributor I

Hi!
I thought no one would answer!
The serial baud for RC663 is 115200!

0 件の賞賛
返信

2,212件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

 

It is not normal.

I would suggest you check the serial connection or the baud rate, default baud for RC663 is 115200.

 

Regards

Daniel

0 件の賞賛
返信