AES CTR on SE050

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AES CTR on SE050

2,425件の閲覧回数
ethanlooney
Contributor II

Hi, I am currently working on a project using AES CTR on the SE050 board. I am using the "sss_cipher_ctypt_ctr" function for this. The function seems to work for the first run, but fails to run properly and produce the desired output on the next runs using the same context. 

When looking at the documenation and demos, I am unable to find any example code using this function. Do you have any example code or other projects that I could look at to get a better understanding of the "sss_cipher_ctypt_ctr"  function?

Thank you. 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,415件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @ethanlooney ,

 

Would you please specify the MW version for SE050? Thanks for your patience!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,406件の閲覧回数
ethanlooney
Contributor II

Hi Kan,

I am currently running release v03.00.05.

Thank you,

Ethan

0 件の賞賛
返信

2,386件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @ethanlooney ,

 

Thanks for the information! I am wondering if you use the same parameters for the next run with "sss_cipher_ctypt_ctr" function , is it possible to share any code snippet for this function? We may try to reproduce this issue here.

 

Thanks for your patience!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信