A5000 RFU pins - inconsistent guidance in datasheet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A5000 RFU pins - inconsistent guidance in datasheet

Jump to solution
1,835 Views
michaelh2
Contributor I

I am replacing the SE050 with A5000 on my schematic. The NXP documentation mentions the parts are pin-to-pin compatible.

However, the Pin Description table of the datasheets for the two parts differ when describing the RFU pins (originally used for ISO 7816 interface):

  • A5000 datasheet (Rev 1.2) recommends
    • pin 3 and 13 to VCC
    • pin 14 to VSS
    • pin 16 to VIN
  • SE050 datasheet (Rev 3.7) recommends
    • pin 3, 13, and 16 NC
    • pin 14 to VSS or VCC

Which one is correct? Ideally I'd like to NC as many pins as possible to simplify layout routing.

Labels (1)
0 Kudos
Reply
1 Solution
1,824 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @michaelh2 ,

 

Please following the SE050 datasheet (Rev 3.7) recommendation, and the data sheet of A5000 will be updated accordingly in the future.

 

Sorry for the confusion that has caused.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,825 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @michaelh2 ,

 

Please following the SE050 datasheet (Rev 3.7) recommendation, and the data sheet of A5000 will be updated accordingly in the future.

 

Sorry for the confusion that has caused.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply