SM1.DCF_CLIENT_TVF and SM1.PARITY implementation if no Custum Parameters are set

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SM1.DCF_CLIENT_TVF and SM1.PARITY implementation if no Custum Parameters are set

619 Views
FabioG
Contributor III

Hi There,

I would to know if these SMs have to be considered if no user parameters are put in DCF and no modification to NxP Factory DCF are done (Product: S32K344). 

Best regard

Fabio 

0 Kudos
1 Reply

572 Views
Yashwant_Singh
NXP Employee
NXP Employee

Hello,

Yes these mechanisms have to be considered. The NXP Factory DCF settings also contain certain safety related data which is protected using these mechanisms. For more details on the DCF data please refer the S32K3xx_DCF_Client attachment of the Reference Manual.

Thanks!

-Yashwant

0 Kudos