SBC MC33907_8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SBC MC33907_8

1,947 次查看
sagarmahajan
Contributor II

Does anyone have the algorithm that MC33907_8 (SBC) uses for LFSR calculation? I have simplified the (NOT(((LFSR x 4)+6)-4))/4 algorithm to be FF – X. In the image attached below, B2 is the default seed that SBC initializes with. To that, controller unit has to reply with 4D (which is FF – B2). In response to that, the SBC generates a random number (64 in this vase). Controller responds it with 9B (FF – 64) and then SBC generates another random number C8. I collected few samples and found out that it basically subtracts the LFSR number generated by SBC and the number that the controller answers. I mean B2 – 4D = 65. 64 – 9B = C9, 91 – 6E = 23, if you follow the numbers shown in the image, I am sure that it generates the random number by subtracting the 2 LFSR values. But that differs by 1 in some cases. In some cases, the next LFSR value is simply the (LFSR_SBC – LFSR_Controller) while in some cases it is (LFSR_SBC – LFSR_Controller – 1).

I am just not able to figure out when they subtract 1 and when they do not. I want to predict the next number generated by SBC. Please check the below image. Left side values are the one generattted by the SBC chip. And right hand side values are what controller has to answer in response to that.

标签 (1)
标记 (1)
0 项奖励
2 回复数

1,804 次查看
maximeclairet
NXP Apps Support
NXP Apps Support

For safety reason, the WD answer formula should not be simplified and the complete calculation should be done by the MCU to guarantee the maximum Diagnostic Coverage (DC) of the WD safety mechanism.

In order to do the correct calculation, the MCU shall use unsigned integer operation on minimum 16 bits register to take into account the carry over.

You can also download the example driver code at https://www.nxp.com/webapp/Download?colCode=MPC5744P-MC33907-MC33908-DEMO&appType=license&location=n...

1,804 次查看
sagarmahajan
Contributor II

Thank you!!! Maxime.

0 项奖励