S32K3xx - SM4, SAF, and ASIL-B vs ASIL-D mechanisms

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3xx - SM4, SAF, and ASIL-B vs ASIL-D mechanisms

50件の閲覧回数
nsiegel
Contributor V

Hi Safety team,

We have a major mm customer using the S32K341/311, and have asked additional Safety Manual questions.  They are developing both ASIL B and ASIL D applications:

Q1:  For AOU_GEN_FOLLOW_ARM_M7_DOC, can you confirm the text "this chip's Safety Manual" is referring to the Arm Cortex-M7 Safety Manual or the safety manual of the S32K3xx?

Q2:  What is comm safe prot (like in SM4.COMM_SAFEPROT)?  Customer cannot find information about this.

Q3: Is it possible to clarify which SMs and AoU are exclusive to ASIL D, and which are also necessary for ASIL B?

Q4:  The  documentation for SM2 shows that SAF mechanisms are relevant for variant S32K311, which is ASIL B. Why is SAF needed for this chip if SAF is targeting ASIL D only?

Q5:  The documentation for SM2 shows that SAF mechanisms bring DC of associated failure modes to 90%. What happens if these SAF mechanisms, DC goes down to 60% (acceptable for ASIL B) or 0% (which would be a gap for ASIL B)?

 

Thanks!

タグ(1)
0 件の賞賛
0 返答(返信)