Master Core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Master Core

Jump to solution
995 Views
HeebeomPark
Contributor II

For the following assumption requirement, master safety core is used , which is Core 2.
However Core 2 is aligned with Lockstep(Core1) and it is more secured. So instead of using Core 2, can Core 0 is used for the following requirement?

 

Software assumption
The application software running on the master safety core manages the FCCU failure status and interrupts.

Rationale
Ensures consistency with the safety concept.

Recommendation
NXP solution: Use the S32 Safety Software Framework (eMCEM module).

0 Kudos
1 Solution
781 Views
john_floros
NXP Employee
NXP Employee

Hello,

It is appropriate to use Core0 as the master safety core as long as it is in lockstep with Core1 on the S32k388.

Regards,

John

View solution in original post

0 Kudos
1 Reply
782 Views
john_floros
NXP Employee
NXP Employee

Hello,

It is appropriate to use Core0 as the master safety core as long as it is in lockstep with Core1 on the S32k388.

Regards,

John

0 Kudos