S32V234 CMU Clock Coverage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32V234 CMU Clock Coverage

跳至解决方案
1,255 次查看
jianlongzhang
NXP Employee
NXP Employee

Hi, 

I would like to ask the clock coverage of S32V234 CMU module. From Table 22-5 of RM, CMU covers only some of the clocks. How to monitor other clocks who doesn't have build-in CMU, for example, QSPI_CLK, CORE_CLK, etc? 

pastedImage_1.png

pastedImage_2.png

Regards

Tony Zhang

1 解答
1,227 次查看
aarul
NXP Employee
NXP Employee

Hi Tony

The Clock monitors are put on all clock nodes based on clock architecture analysis and safety requirements derived from assumed safety concept. Some reasons for this are:

1. There is already a branch of clock that is monitored which offers adequate coverage. (eg: core_clk monitored via sys clock)

2. There are additional safety mechanisms that offer adequate coverage. (eg: core clock failure leading to malfunction in cores which will cause WDOG failure or CRC mismatch for data transfer through Quadspi)

3. Some modules are not safety related (eg: debug) and so do not need in-field protection.

Hope this helps,

Regards

-Aarul

在原帖中查看解决方案

2 回复数
1,228 次查看
aarul
NXP Employee
NXP Employee

Hi Tony

The Clock monitors are put on all clock nodes based on clock architecture analysis and safety requirements derived from assumed safety concept. Some reasons for this are:

1. There is already a branch of clock that is monitored which offers adequate coverage. (eg: core_clk monitored via sys clock)

2. There are additional safety mechanisms that offer adequate coverage. (eg: core clock failure leading to malfunction in cores which will cause WDOG failure or CRC mismatch for data transfer through Quadspi)

3. Some modules are not safety related (eg: debug) and so do not need in-field protection.

Hope this helps,

Regards

-Aarul

1,227 次查看
jianlongzhang
NXP Employee
NXP Employee

Hi Aarul

Thanks for your comments. I think it is reasonable. 

0 项奖励