S32 Safety Software Framework (S32 SAF) Safety Manual

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 Safety Software Framework (S32 SAF) Safety Manual

跳至解决方案
3,926 次查看
sazad
Contributor I

The S32G safety manual refers to a document called "S32 Safety Software Framework (S32 SAF) Safety Manual".

Where can I access this document?

0 项奖励
1 解答
3,910 次查看
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

I uploaded it into your support case Files.

在原帖中查看解决方案

0 项奖励
9 回复数
3,913 次查看
sazad
Contributor I

Hi Martin,

I need to get the SAF safety Manual reviewed by my software team before we finalize the socket with S32G. Its difficult to make large decisions without full due-diligence. Can you please suggest how we can get access to this document?

Thanks

Sarosh

 

0 项奖励
3,911 次查看
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

I uploaded it into your support case Files.

0 项奖励
3,923 次查看
martinkaspar-r3
NXP Employee
NXP Employee

The S32G SAF Safety Manual is included in the SAF SafetyPack which is delivered together with the S32G SAF product.

0 项奖励
3,859 次查看
hunterxiao
Contributor II

Hello Martin, 

Nio need to read S32 Safety Software Framework user manual with internal software team together.  detailed technical report is in need before purchase  request. 

please send me firstly.

Thanks 

Hunter Xiao  

0 项奖励
3,847 次查看
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

the basic information can be found in the Product Briefs: S32 Safety Software Framework (SAF) | NXP Semiconductors

There is available the Evaluation version of the SAF product with the full documentation, but with highly reduced functionality. The purpose is exactly the evaluation before the purchase. Please, contact the NXP Sates/Marketing to obtain the access to such version.

3,818 次查看
hunterxiao
Contributor II

Hello Martin,

                When I tried to review S32Gxxx reference manual, I found that the safety HW SM related registers recommended values are need to contact NXP to get. Please see an example screen shot below as highlighted as yellow.

Could you please share all HW SM feature configuration register recommended values sheet with explanation how to select those configuration?

LBIST  register.jpg

Thank you very much!

Hunter Xiao

 

 

0 项奖励
3,808 次查看
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

the SELFTEST_GPR registers are initialized by the Bist driver (so the values for these registers are delivered as part of the Bist driver code as only the Bist driver shall be used to run a selftest). The Bist driver is part of the SPD (Safety Peripheral Drivers) release package or also SAF (Safety Software Framework package) available for download from nxp.com.

Note that in SCTU2 section in HW reference manual there is documented the following which is valid also for SELFTEST_GPR:

BIST.jpg

3,798 次查看
hunterxiao
Contributor II

Hello Martin,

Thanks for reply!.Could you please share S32G HW reference manual document name?  

I guess this document could tell  HW safety register recomended with explaining.

Have a nice day!

Hunter Xiao

标记 (1)
0 项奖励
3,768 次查看
martinkaspar-r3
NXP Employee
NXP Employee

The document name is S32G3 Reference Manual

S32G2 Reference Manual (nxp.com)

0 项奖励