FMEDA DCMPF calculation question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FMEDA DCMPF calculation question

898 Views
peter793731677
Contributor I

I am doing a system level FMEDA. When reading S32K146 MCU FMEDA, I can't understand the DCSPF and DCMPF provided in the report. I try to re-calculate it and put these numbers in column L and M.  I use following formulas:

DCSPF=(λSR-(λSPFRF))/λSR

DCMPF=(λSR-(λSPFRF)-λMPF_undet)/(λSR-(λSPFRF))

Could you please help to point out where is my mistake?

peter793731677_3-1630397394986.png

 

 

 

 

0 Kudos
1 Reply

889 Views
ehtesham_khan
NXP Employee
NXP Employee

Hi Peter,

The S32K146 is ASIL-B target MCU. Here we limit the values of DCSPF and DCMPF less than that of ASIL-C to make sure that the S32K146 should not be used as the ASIL-C or higher.
The formulas you used to get these numbers are correct.

0 Kudos