FMEDA DCMPF calculation question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FMEDA DCMPF calculation question

961件の閲覧回数
peter793731677
Contributor I

I am doing a system level FMEDA. When reading S32K146 MCU FMEDA, I can't understand the DCSPF and DCMPF provided in the report. I try to re-calculate it and put these numbers in column L and M.  I use following formulas:

DCSPF=(λSR-(λSPFRF))/λSR

DCMPF=(λSR-(λSPFRF)-λMPF_undet)/(λSR-(λSPFRF))

Could you please help to point out where is my mistake?

peter793731677_3-1630397394986.png

 

 

 

 

0 件の賞賛
1 返信

952件の閲覧回数
ehtesham_khan
NXP Employee
NXP Employee

Hi Peter,

The S32K146 is ASIL-B target MCU. Here we limit the values of DCSPF and DCMPF less than that of ASIL-C to make sure that the S32K146 should not be used as the ASIL-C or higher.
The formulas you used to get these numbers are correct.

0 件の賞賛