Debug mode disable in MPC5746C SM: SM_047

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug mode disable in MPC5746C SM: SM_047

ソリューションへジャンプ
888件の閲覧回数
BoxLi
NXP Employee
NXP Employee

Hi

I saw there is a statement in MPC5746C Safety Manual Rev2: SM_047''Assumption:[SM_047] Debugging will be disabled in the field while the device is being used for safety-relevant functions. [end]"

My question is how to implement this. There is no detail description here.

I saw in MPC5746R or MPC5744P SM, JCOMP should be pulled high and monitored by FCCU. 

Can you help check and clarify this issue? Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
1 解決策
862件の閲覧回数
aarul
NXP Employee
NXP Employee

Hi Box Li

This is correct. For fulfilling this assumption:

JCOMP should be pulled low and monitored by FCCU

Regards

-Aarul

PS: Correction Made on pull on JCOMP. JCOMP should be pulled to the value that ensures that the TAP controller is in reset state in field.

元の投稿で解決策を見る

0 件の賞賛
1 返信
863件の閲覧回数
aarul
NXP Employee
NXP Employee

Hi Box Li

This is correct. For fulfilling this assumption:

JCOMP should be pulled low and monitored by FCCU

Regards

-Aarul

PS: Correction Made on pull on JCOMP. JCOMP should be pulled to the value that ensures that the TAP controller is in reset state in field.

0 件の賞賛