uart demo not working as expect.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

uart demo not working as expect.

666 次查看
BingBai_S
Contributor I

Dear all, 

I’ve been trying to run the PDK Uart demo on the  S32Z2 S32Z280-400 EVB board. So far, the configuration and build went smoothly, no errors at all.
 
But I hit a little snag: when I launch the demo with the NXP Debug probe, the app itself starts up fine, but there’s no output at all on the serial console. I even tried typing “Hello” into the console to test the interaction, and the app didn’t respond either.
 
Wondering if anyone here has run into a similar issue, or if you have any troubleshooting tips I could try?
 
Quick heads-up on my setup: I’m using S32 Design Studio 3.6.2, and the board’s connected to my PC directly with a USB-A cable.
 
Thanks a ton for your help!

 

标记 (1)
0 项奖励
回复
3 回复数

607 次查看
BingBai_S
Contributor I

I use S32Z/E PDK version 3.6.0, meanwhile I have tested the semihosting functions, not output anything, when I try to printf() something.

0 项奖励
回复

580 次查看
Joey_z
NXP Employee
NXP Employee

Hi,BingBai_S

Thank you for your reply.

Do you use the demo of Uart_Example_S32Z2XX_R52?

BR

Joey

0 项奖励
回复

622 次查看
Joey_z
NXP Employee
NXP Employee

hi,BingBai_S

Which version of RTD are you using? and are you using the demo of Uart_Example_S32Z2XX_R52 ?

BR

Joey

0 项奖励
回复