S32E288 Failure during execution of python script

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32E288 Failure during execution of python script

1,764 Views
cszhang
Contributor II

Hi Nxp experts,

I created a new S32E288 M33 project on S32 Design Studio for S32 Platform Version: 3.6.7, then built and try to run it on S32 Debugger,

cszhang_2-1778704023580.png

but i got 

cszhang_4-1778704082217.png

Please help me understand what caused the issue.

Thanks

 
 

 

 

 

 

Tags (1)
0 Kudos
Reply
6 Replies

1,727 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @cszhang,

Thanks for reaching out to us. About your problem, could you let me know the RTD version your are using? and if you can debug any of the examples?

 

Thanks. 

0 Kudos
Reply

1,696 Views
cszhang
Contributor II

The RTD is

cszhang_0-1778766644319.png

and I tested <Siul2_Dio_Ip_Example_S32E2XX_R52> too, got the same issue. Then I clicked the <Test Connection> on Debugger tab,  the SIul2 example project did the configuration generation. measured JTAG VTREF value, it's 3.297 V.

cszhang_1-1778766751847.png

cszhang_0-1778767016041.png

 

the E2 to JTAG connector, has a 33-ohm resistor on board,

cszhang_2-1778766847722.png

 

 

 

0 Kudos
Reply

1,676 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @cszhang,

Thanks for all the information. I will need to check if S32DS 3.6.7 works with RTD 2.0.1, the official supported version is 3.6.1:

alejandro_e_0-1778812075407.png

 

However, following the AN12530, using 33 ohm resistors is not the best approach, the recommended connections shown in section 7 Example schematics show 0 ohm resistors in series:

alejandro_e_1-1778812231629.png

Please try using 0 ohm resistors and let me know if the behavior changes.

If the problem persists, please share the state of the BOOTMOD pins in your board.

 

Thanks.

 

 

 

0 Kudos
Reply

1,666 Views
cszhang
Contributor II
Thanks for the quick response, my coworker is looking into hardware, now seems the FS86 PMIC works not well.
0 Kudos
Reply

1,653 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello again @cszhang,

You can check our recommendations for the FS86 in section 3.1 Power supply recommendation of the S32E HW Design Guidelines, also you can see how the S32E EVB is using the FS86 in the Design Files for the S32E288-975EVB.

Note that the design files are missing the schematics pdf, if you require that file please open a private support ticket using the following steps Tutorial for NXP Support Case Portal. If you do so please include the link to this post and my username so that we ensure I handle the ticket, then I can send you the file.

 

In any case, please let me know if I can help you with anything else.

 

0 Kudos
Reply

1,268 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello again @cszhang,

Were you able to overcome the problem with the PMIC? From my side I was able to debug the Siul2_Dio_Ip_Example_S32Z2XX_SMU sample project in S32DS 3.6.7, using a S32Z280-594EVB. Therefore the software environment should not represent a problem.

In any case, let me know if I can help you with anything else.

 

Regards. 

0 Kudos
Reply