FlexLLCE example stuck in CAN initialization

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FlexLLCE example stuck in CAN initialization

7,292 次查看
carmelom
Contributor I

We’re currently integrating the FlexLLCE example provided for the S32E R52 core on GHS u-velOSity and have encountered a high-priority issue during execution:

The function Can_43_FLEXLLCE_SetControllerMode(Controller=0, Transition=CAN_CS_STARTED (1)) (see attached mainLLCE) does not return, as it gets stuck in a loop within Can_43_FLEXLLCE_Ipw_MainFunction_Mode, located in Can_43_FLEXLLCE_Ipw.c at line 1082, column 16 (refer to the attached Block_function_LLCE and CS_FLEXLLCE_example).

 

It appears that the selected controller never transitions to the CAN_STARTED state.

 

All prior initialization functions complete successfully and do not indicate any errors.

Please note that the LLCE firmware was compiled according to the provided instructions related to our (GHS) complier. However, we are not using your default startup code, we are instead using the startup.c file attached.

BLOCKING FUNCTION

blocking functionblocking function

MAIN

mainmain

STARTUP CODE

#include <S32Z2_MSCM.h>

int Sys_GetCoreID(void)
{

return (IP_MSCM->CPXNUM & MSCM_CPXNUM_CPN_MASK);

}

CALL STACK

0 Can_43_FLEXLLCE_Ipw_MainFunction_Mode(Can_pControllerConfig=0x3230be74, Can_pControllerState=0x3232363c) [demos/FlexLLCE_example_routing_S32Z2XX_R52/RTD/src/Can_43_FLEXLLCE_Ipw.c:1082,16]
1 Can_43_FLEXLLCE_Ipw_SetControllerToStartMode(Can_pControllerConfig=0x3230be74) [demos/FlexLLCE_example_routing_S32Z2XX_R52/RTD/src/Can_43_FLEXLLCE_Ipw.c:615,38]
2 Can_43_FLEXLLCE_SetControllerMode(Controller=0, Transition=CAN_CS_STARTED (1)) [demos/FlexLLCE_example_routing_S32Z2XX_R52/RTD/src/Can_43_FLEXLLCE.c:1164,32]
3 main(argc=1, argv=0x323a7dc0) [demos/FlexLLCE_example_routing_S32Z2XX_R52/src/main.c:138,10]

 

标记 (1)
0 项奖励
回复
12 回复数

7,215 次查看
carmelom
Contributor I

Could this issue be related to the fact that our startup code is not starting the M33 core on which the LLCE firmware is supposed to run?

0 项奖励
回复

7,202 次查看
carlos_o
NXP TechSupport
NXP TechSupport

Hi @carmelom,

Thanks for your questions

Could you please verify that in your project -> properties -> Resource -> Linked Resources the name FLEXLLCE_BIN_DIR has the value of the directory where the binaries of the FLEXLLCE package are located?

Also, could you verify or share your clock configuration?

 

 

0 项奖励
回复

7,183 次查看
carmelom
Contributor I

Hello @carlos_o 

Thank you for your answer!

Regarding the firmware, we are porting the example on our toolchain and I created a gpj file to include the content of FLEXLLCE_BIN_DIR in the program. it includes both c files and firmware folders (we are using ghs folder). 

Regarding the clock configuration I can share the files generated on s32ds. Could you suggest the right way to share them? Since there is the NXP copyright I don't believe I can share them here. However I left all the configurations as they were in the provided example

Thank you 

Carmelo Maniscalco

 

 

0 项奖励
回复

7,165 次查看
carlos_o
NXP TechSupport
NXP TechSupport

Hi @carmelom,

Thanks for sharing the information.

If the clock config is as the example there is not needed to be shared, thank you.

Could you please provide which version of the FLEX LLCE are you using?

I tried to reproduce the issue with the 0.9.3 but I'm not having any issue. 

Also, please provide which version of RTDs are you using?

 

 

0 项奖励
回复

7,156 次查看
carmelom
Contributor I

Hello  @carlos_o 

FlexLLCE version 0.9.3 and RTD version 2.0.0

So maybe, as I already wrote the issue is related to the startup code? since we are using a different one. Maybe we are not correctly initializing the system. Do you have a startup code that can be built with GHS compiler?Please consider that is you have that, we could solve others issue we have on other examples 

Thank

Carmelo

0 项奖励
回复

7,141 次查看
carlos_o
NXP TechSupport
NXP TechSupport

Hi @carmelom,

I review the startup code that is given with the example, it has llce CRAM and DRAM initialization. The startup code the examples has is standard C and assembly. Could you try to use this code with the GHS compiler? 

 

 

0 项奖励
回复

7,117 次查看
carmelom
Contributor I

Hello @carlos_o 

I took the startup code provided in the folder C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32ZE\RTD\Platform_TS_T31D53M20I0R0 that contains files already written for ghs compiler and I modify our ld file to have both sections  for u-velOSity and RTD drivers. The result is that the program is stuck as before.

How I can check CRAM and DRAM initializations are correctly done?

Thank You

Carmelo Maniscalco

0 项奖励
回复

7,112 次查看
carlos_o
NXP TechSupport
NXP TechSupport

Hi @carmelom 

The FlexLLCE example have their own startup code at C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32ZE\FLEXLLCE\Can_43_FLEXLLCE_TS_T31D53M9I3R0\examples\S32DS\FlexLLCE_example_routing_S32Z2XX_R52\Project_Settings\Startup_Code this route is the default path.

In the core.c file the CRAM and DRAM for FlexLLCE are initialized in the function Core_MPU_Init at the loop with the rbar and rlbar variables

carlos_o_0-1750979103867.png

There is the write_PRBAR (assembly function) initialize it.

 

0 项奖励
回复

6,973 次查看
carmelom
Contributor I

Hello @carlos_o

Integrating the startup code provided with the example the issue is still there.

Any other idea or code portion to debug to understand why the example is not working?

Thank you

Carmelo

0 项奖励
回复

6,910 次查看
carlos_o
NXP TechSupport
NXP TechSupport

Apologies for the late response, 

Could you confirm that the example is stuck in the same line?

Are you able to run other examples successfully? 

 

0 项奖励
回复

6,907 次查看
carmelom
Contributor I
破坏者
Hello @carlos_o ,

Yes, it ends in the same point and I am able to run multiple examples integrated on u-velOSity e.g FlexCAN, SiulPort, NETC etc...

Are you sure the Flex LLCE example can be run on GreenBox3 as it is?


Thank You
Carmelo


0 项奖励
回复

6,888 次查看
carlos_o
NXP TechSupport
NXP TechSupport

Hi @carmelom

I tried to run the example at my end (I only have the option to compile with gcc) and the example works as expected. 


0 项奖励
回复