Change boot core of the examples for S32Z2/E2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Change boot core of the examples for S32Z2/E2

Change boot core of the examples for S32Z2/E2

This document offer guide for modifying the boot core configuration of various example projects provided for the S32Z/E family. In the default setup, many S32E examples are configured to run on the Cortex-R52 cores, while S32Z examples are designed to run on the SMU (System Manager Unit) core.

As a specific case, this guide outlines the steps required to modify the Dio_Example_S32E2XX_R52 project to run on the SMU (System Manager Unit) core. Although this document focuses on a single example, the same approach can be applied to other examples provided by NXP

附件
无评分
版本历史
最后更新:
3 周之前
更新人: