eFuse Address Region in the Memory Map

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eFuse Address Region in the Memory Map

ソリューションへジャンプ
5,319件の閲覧回数
partharoy
Contributor II

Hello Support,

In the S32V234 Reference Manual, I am unable to find the address region for eFuse area.

Can you please provide me the details?

Also, is there any documents available about how to program the eFuse as in the Reference Manual I am unable to find anything.

Thank you.

1 解決策
4,947件の閲覧回数
marie-annelemen
NXP Employee
NXP Employee

Hello Partha,

The fuses are part of the module called OCOTP (On-Chip One Time Programmable) controller which is based at the address 0x4005F000 (indicated in the memory map spreadsheet). You will find the description of the fuses inside the module chapter and in the "Fuse Map" excel spreadsheet, attached to the reference manual.
The OCOTP chapter also describe how to fuse the part.

Marie-Anne

元の投稿で解決策を見る

2 返答(返信)
4,947件の閲覧回数
sunghwanpark
Contributor II

Hello Partha,

 

If you have been contracted to NXP, you only have to ask NXP below.

1. If you need to know fuse operations and configurations.
 (1) Require the S32V234RM(Reference Manual)
     - Normally, it's a S32V234RM_Rev(X).(Y).pdf
 (2) Through this RM document,
    - You can see the fusing operation through OCOTP chapter.
    - Also, you can see a fuse map including bit positions via the S32V234_FuseMap.xlsx(the attached fuse map sheet in the S32V234RM)

2. If you want to make a fuse program.
 (1) Require the fuse application.
    - If you want to do it yourself with RM document, you need to know about some registers(especially MC_ME) how to set for fusing operation(E.g. Mode setting, XOSC, PLL, Clock, Shadow register, ECC calculate, etc.) but it is not as easy as you think.

 

I hope this will help.

4,948件の閲覧回数
marie-annelemen
NXP Employee
NXP Employee

Hello Partha,

The fuses are part of the module called OCOTP (On-Chip One Time Programmable) controller which is based at the address 0x4005F000 (indicated in the memory map spreadsheet). You will find the description of the fuses inside the module chapter and in the "Fuse Map" excel spreadsheet, attached to the reference manual.
The OCOTP chapter also describe how to fuse the part.

Marie-Anne