Yocto S32V Kernel Panic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto S32V Kernel Panic

4,021件の閲覧回数
hennadiyyatskov
Contributor I

We are currently building the BSP 15 for the S32V. The Yocto build is successfull and we can boot from the generated image. However during boot, we get a kernel panic, the init script simply fails with an error (-2).

I've attached the latest bootlog, were I tried to start init directly using init=/sbin/init.sysvinit, sadly the result is the same as for init=/sbin/init

ラベル(1)
0 件の賞賛
返信
1 返信

3,669件の閲覧回数
KushalShahNXP
NXP Employee
NXP Employee

Hi Hennadiy,

Did you used correct components from the Yocto build? I mean u-boot, dtb file, rootfs, image.

Please use the latest BSP available (now v16.1) and try again.

Thanks,

Kushal

0 件の賞賛
返信