Which interface(s) can I use to program the eMMC ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which interface(s) can I use to program the eMMC ?

2,630 Views
tomlowdermilk
Contributor I

I'm planning to use S32V234 and boot from eMMC. However, which interface or interfaces can I use to program the eMMC? Is it JTAG or some other interface?

0 Kudos
Reply
1 Reply

2,494 Views
KushalShahNXP
NXP Employee
NXP Employee

Hi Tim,

One of the methods can be loading via network.

Please follow the steps described in Section 3.1.2 Setup eMMC memory of Linux BSP Reference manual for detailed instructions.

Regards,

Kushal

0 Kudos
Reply