S32V234 Processor Temperature Sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32V234 Processor Temperature Sensor

3,726 Views
sriramanravi
Contributor I

Hi,

We are using S32V234 Processor from NXP and are trying to read the temperature Sensor Values. It will be helpful if any one can provide any input on how to read Temperature Sensor Values for S32V234 on chip Temperature Sensor in U-Boot or Linux, is there already a driver for that?

Best Regards

Sriraman Ravi

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

3,366 Views
tommalnar
Contributor III

For Linux there is a driver available at \drivers\thermal\s32v234_thermal.c as part of the kernel used in BSPv14.

0 Kudos
Reply

3,366 Views
rajeevr
Contributor I

Hi All,

Anyone knows the answer for the above question. Please reply it would be helpful.

0 Kudos
Reply