Read CAN-FD Using S32V234 Transceivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Read CAN-FD Using S32V234 Transceivers

3,961 Views
christharp
Contributor I

Hello,

I am trying to read in CAN FD data using S32V234 CAN transceivers on BlueBox via SocketCAN.

So far, I have been able to:

  • Read and write non-FD CAN data using both CAN0 and CAN1 transceivers.
  • Use cangen to generate FD traffic on a virtual CAN vcan0

However, when I try to read FD data using either CAN0 or CAN1, I run into issues.

Specifically, when I try to set the interface to FD, I receive the message "RTNETLIINK answers: Operation Not Supported".

            example command -> $sudo ip link set can0 up type can bitrate 500000 dbitrate 2000000 fd on 

I had seen this link, indicating a similar issue: Access CAN-FD on S32V234 

Based on the response, I have read through the BSP documentation, but I don't see any specific references to FD.

Could anyone help with this?

Any help would be appreciated.

Thanks,

Chris

0 Kudos
Reply
1 Reply

3,646 Views
KushalShahNXP
NXP Employee
NXP Employee

Hi Chris,

We have stopped supporting this community. But we still support S32V2 question using our ticketing system.

Please create the request at www.nxp.com/support using Support Requests option. Our experts will help you.

Thank you for understanding.

Regards,

Kushal

0 Kudos
Reply