EEPROM device connecting via SPI interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EEPROM device connecting via SPI interface

4,629件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

We would like to use the EEPROM device (P/N S25A080A) via SPI interface of S32V234.

Can S32V234 support device which using more than 32bits CMD?


Because, S25A080A is using 8, 16, 32 and more than 32bits CMD.

therefore, I worry about CMD FIFO can not support more than 32bits CMD.

Best Regards,

Kazuma Sasaki.

タグ(1)
0 件の賞賛
返信
1 返信

4,404件の閲覧回数
KushalShahNXP
NXP Employee
NXP Employee

Thanks for posting question. But we are now moving to ticketing system to support this device. This community will be closed soon.

So, I would encourage to raise a service request at www.nxp.com/support using "Support Requests" option and experts will help you with your questions.

 

-Kushal

0 件の賞賛
返信