EEPROM device connecting via SPI interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EEPROM device connecting via SPI interface

1,905 Views
Kazuma_Sasaki
Senior Contributor I

We would like to use the EEPROM device (P/N S25A080A) via SPI interface of S32V234.

Can S32V234 support device which using more than 32bits CMD?


Because, S25A080A is using 8, 16, 32 and more than 32bits CMD.

therefore, I worry about CMD FIFO can not support more than 32bits CMD.

Best Regards,

Kazuma Sasaki.

Tags (1)
0 Kudos
Reply
1 Reply

1,680 Views
KushalShahNXP
NXP Employee
NXP Employee

Thanks for posting question. But we are now moving to ticketing system to support this device. This community will be closed soon.

So, I would encourage to raise a service request at www.nxp.com/support using "Support Requests" option and experts will help you with your questions.

 

-Kushal

0 Kudos
Reply