APECV gftt corner detector error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

APECV gftt corner detector error

2,862 Views
xuewong
Contributor I

Hello,

I am currently trying to use good feature to track corner detector from apexcv in one of my project. I was able to call Initilize() and Process() function without error code return (these functions always return 0). However inside the Process() function, i got the following message:

ACF_PROCESS_APU::SelectScenario_internal() -> A suitable scenario could not be found

ACF_PROCESS_APU::Wait() -> process was never started (i.e. nothing to wait for)

After reading the source code of acf_process_apu, its appear that this error is related to the setting of chunkWidth and chunkHeight. However, i did not see any function that allow me to configure them. 

The input image is a gray scale image with size 1280x800. I also tried different image size, but they are all returning same error message. 

Thanks you

0 Kudos
Reply
1 Reply

2,683 Views
KushalShahNXP
NXP Employee
NXP Employee

Hi Xue,

Please raise the ticket at www.nxp.com/suport using "Service Request" for support on this.

-Kushal

0 Kudos
Reply