Physical parameters of FC-BGA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Physical parameters of FC-BGA

ソリューションへジャンプ
4,610件の閲覧回数
eugene_shatlov
Contributor I

Hi. What are the physical parameters of FC-BGA 621? This is packege for S32v234, i read two datasheets and can't understand how to draw a physical model S32v234 in Altium Designer. In 1st file says -"21x21 mm" , 2 - "17x17". 
Do you have detailed specifications or a scheme with dimensions (the distance between the pins and their location). 
Thanks an advance)

Eugene.

タグ(2)
1 解決策
4,358件の閲覧回数
KushalShahNXP
NXP Employee
NXP Employee

Hi Eugene, 

The first you attached is the S32V234.pdf is the datasheet. Please follow the datasheet for the up-to-date information. It also points to document 98ASA00819D for package drawing. This document can be found here: https://www.nxp.com/docs/en/package-information/98ASA00819D.pdf?fsrch=1&sr=1&pageNum=1

Regards,

Kushal

元の投稿で解決策を見る

1 返信
4,359件の閲覧回数
KushalShahNXP
NXP Employee
NXP Employee

Hi Eugene, 

The first you attached is the S32V234.pdf is the datasheet. Please follow the datasheet for the up-to-date information. It also points to document 98ASA00819D for package drawing. This document can be found here: https://www.nxp.com/docs/en/package-information/98ASA00819D.pdf?fsrch=1&sr=1&pageNum=1

Regards,

Kushal