whether S32K144 PTC3, PTC2 pin have LPUART0 function?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

whether S32K144 PTC3, PTC2 pin have LPUART0 function?

ソリューションへジャンプ
3,649件の閲覧回数
hansonhe
NXP Employee
NXP Employee

     Dear, We see from ON77P version RM as below, PTC3,PTC2 do not have LPUART0 function

 

、pastedImage_1.png

 

But for the latest S32K RM from official web, it say that we need double check IO Signal Description Input Multiplexing sheet(s),

 

pastedImage_2.png

 

We could see that PTC2,PTC3 could support uart feature as below, could you help check whether S32K144 PTC3, PTC2 pin have LPUART0 function?

 

pastedImage_3.png

 

0 件の賞賛
返信
1 解決策
3,358件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

0N77P is  cut 1.0 and I recommend you to not use this cut. Use cut 2.0 (0N47T), which is newer and many things are fixed there. Reference manual for S32K placed at NXP website is determined for the newer cut (0N47T) and this supports LPUART at PTC2/PTC3.

Regards,

Martin

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,358件の閲覧回数
hansonhe
NXP Employee
NXP Employee

Dear,

Do you have some update about this?

0 件の賞賛
返信
3,359件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

0N77P is  cut 1.0 and I recommend you to not use this cut. Use cut 2.0 (0N47T), which is newer and many things are fixed there. Reference manual for S32K placed at NXP website is determined for the newer cut (0N47T) and this supports LPUART at PTC2/PTC3.

Regards,

Martin

0 件の賞賛
返信
3,358件の閲覧回数
hansonhe
NXP Employee
NXP Employee

Dear, 

Current S32K  0N47T have below bug for LPUART0, 

e10656: LPUART: The RXD pin Active Edge Interrupt flash does not assert when active edge is detected.

Whether S32K14x_SDK_EAR_0.8.3  have fixed this bug?

0 件の賞賛
返信
3,358件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

for S32K144 microcontroller there is SDK RTM 1.0.0, so SDK EAR 0.8.3 for S32K144 will not be updated anymore. Please use the RTM 1.0.0.

Regards,

Martin

0 件の賞賛
返信