use internal reference voltage for ADC S32K14X

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

use internal reference voltage for ADC S32K14X

2,120件の閲覧回数
naderkhamess
Contributor III

Hello there,

We are working with MCU S32K14X ADC and we were wondering, is there internally generated reference voltage can be used for vref in the ADC instead of using external vref ? the issue is the external supply is not stable and we need to have stable vref provided internally for the ADC if possible.

if feasible, what are the internal reference voltage options?

Thanks.

Best regards,

Nader Khamess

タグ(3)
0 件の賞賛
返信
1 返信

2,101件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Nader Khamess,

There is no internal reference voltage can be used as ADC VREF.

43.6 ADC Reference Options.png

There is 1V bandgap, but it's ADC input not vref. 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信