PFE-demo problems on S32G274

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PFE-demo problems on S32G274

1,038 Views
nioer
Contributor I

hi, nxp, when i use the PFE demo, there is a lot of problems. 

There is no RTD_1.0.0 of S32G2 M7 driver package, Could you give us a package of RTD_1.0.0 ?

And in the S32G PFE MCAL 4.4 driver - SW32G2XX_MCL01_0.9.6_D2112 there is no related MCAL configuration demos.

nioer_0-1646101989657.png

According to current resources, we could not use the PFE demo. Could you give us some help?

Thank you nxp.

 

 

0 Kudos
Reply
1 Reply

1,003 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello nioer,

There is l2 bridge and router reference code in PFE_MCAL example application.

The demo is enable by setting the make options,“FCI_L2BR_TEST “ and “FCI_RTABLE_TEST”.

Bio_TICFSL_0-1646937945096.jpeg

 

And you can check “FCI_API_Reference.pdf” to do some modifications based on the sample code.

 

Regards

0 Kudos
Reply