use RSA in RTD Crypto_43_HSE module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

use RSA in RTD Crypto_43_HSE module

1,227 Views
BigSun
Contributor II

Hi, I tried to use RSA in RTD Crypto_43_HSE module. but is indicate not supported.

ENV: RTD4.0.0 P04  IDE3.5  EBTREOS29

Error Notes:

category : Error
project : SS11_IBC_S32K312
description: Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Crypto_43_HSE/ELEMENTS/Crypto/CryptoPrimitives/CryptoPrimitives_0/CryptoPrimitive/CryptoPrimitive_SIGNATUREVERIFY/CryptoPrimitiveService": The configured primitive is not in the list of primitives supported by the Crypto driver. When adding the Crypto driver in the configurator, you can choose to use one of the available recommended configurations which will automatically fill the CryptoPrimitives list with all primitives supported by the Crypto driver.
detailed : Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Crypto_43_HSE/ELEMENTS/Crypto/CryptoPrimitives/CryptoPrimitives_0/CryptoPrimitive/CryptoPrimitive_SIGNATUREVERIFY/CryptoPrimitiveService": The configured primitive is not in the list of primitives supported by the Crypto driver. When adding the Crypto driver in the configurator, you can choose to use one of the available recommended configurations which will automatically fill the CryptoPrimitives list with all primitives supported by the Crypto driver.
id : 1019
resource :
path : /AUTOSAR/TOP-LEVEL-PACKAGES/Crypto_43_HSE/ELEMENTS/Crypto/CryptoPrimitives/CryptoPrimitives_0/CryptoPrimitive/CryptoPrimitive_SIGNATUREVERIFY/CryptoPrimitiveService
location :
stack :


category : Error
project : SS11_IBC_S32K312
description: Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Crypto_43_HSE/ELEMENTS/Crypto/CryptoPrimitives/CryptoPrimitives_0/CryptoPrimitive/CryptoPrimitive_SIGNATUREGENERATE/CryptoPrimitiveService": The configured primitive is not in the list of primitives supported by the Crypto driver. When adding the Crypto driver in the configurator, you can choose to use one of the available recommended configurations which will automatically fill the CryptoPrimitives list with all primitives supported by the Crypto driver.
detailed : Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Crypto_43_HSE/ELEMENTS/Crypto/CryptoPrimitives/CryptoPrimitives_0/CryptoPrimitive/CryptoPrimitive_SIGNATUREGENERATE/CryptoPrimitiveService": The configured primitive is not in the list of primitives supported by the Crypto driver. When adding the Crypto driver in the configurator, you can choose to use one of the available recommended configurations which will automatically fill the CryptoPrimitives list with all primitives supported by the Crypto driver.
id : 1019
resource :
path : /AUTOSAR/TOP-LEVEL-PACKAGES/Crypto_43_HSE/ELEMENTS/Crypto/CryptoPrimitives/CryptoPrimitives_0/CryptoPrimitive/CryptoPrimitive_SIGNATUREGENERATE/CryptoPrimitiveService
location :
stack :

BigSun_0-1713842466270.pngBigSun_0-1713842466270.pngBigSun_1-1713842484836.pngBigSun_1-1713842484836.pngBigSun_2-1713842501644.pngBigSun_2-1713842501644.png

 

 

 

 

 

 

 

 
 

 

Tags (1)
0 Kudos
Reply
0 Replies