...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

...

1,931 Views
jebartling
Contributor II

Sent from Mail for Windows 10

I am trying to get the FIRC out to pb5 the following code compiles but traps on the highlighted statement when I try to right the pin mux.

/ port setup

PTB -> PDDR |= 0b10000; //Set PORT B5 to an output register

PORTB-> PCR[0b100000] |= 0b10100000000; //set port function to 5 for clkout function

SCG ->FIRCDIV |= 0b100000000; //Set CLKDIV2 to Divide by 1

SCG-> FIRCCSR |= 0b1001; //Enable FIRC regulator and FIRC

SIM->CHIPCTL |= SIM_CHIPCTL_CLKOUTSEL(0b0110); // select FIRC for input to clkout multiplexor

SIM->CHIPCTL |= SIM_CHIPCTL_CLKOUTDIV(0b101); // set clkout divisor to 6 for 8MHz output

SIM->CHIPCTL |= SIM_CHIPCTL_CLKOUTEN(0b1); // enable clkout

int counter = 0;

for (;;) {

counter++;

counter %= COUNTER_LIMIT;

}

Any suggestions on how to modify this line of code

Jim

0 Kudos
Reply
2 Replies

1,832 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

try to use below code for B5 pin setting

PCC-> PCCn[PCC_PORTB_INDEX] = PCC_PCCn_CGC_MASK; /* Clock for PORT B */
PORTB->PCR[5] = PORT_PCR_MUX(5);  /* Port B5:  MUX = ALT5, CLKOUT */

BR, Petr

0 Kudos
Reply

1,832 Views
jebartling
Contributor II

Here is the trap statement I get when single stepping through the code

Target has been RESET and is active.
BusFault: A precise (synchronous) data access error has occurred.
Possible BusFault location: 0x4004A014.
HardFault: A fault has been escalated to a hard fault.

I am using a s32k144 evb board

0 Kudos
Reply