unexpected interrupt occured when adc conversion not finished yield

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

unexpected interrupt occured when adc conversion not finished yield

1,789件の閲覧回数
eafly
Contributor I

Using Keil + S32K144 sdk pack for keil , configure PTC15/ADC0_SE13/FTM1_CH3/TRGMUX_IN8 PIN as adc input source.
Software interrupt trigger was configured, Here is my question:When software trigger called(adc_start_convert), The unexpected interrupt was trigger. It confused me: Isn't interrupt function called when adc conversion completed?


Initialization:
{
...

PCC->PCCn[PCC_ADC0_INDEX] &= ~PCC_PCCn_CGC_MASK;
PCC->PCCn[PCC_ADC0_INDEX] |= PCC_PCCn_PCS(6); /* PCS=6: 80MHZ */
PCC->PCCn[PCC_ADC0_INDEX] |= PCC_PCCn_CGC_MASK;

ADC0->CFG1 = ADC_CFG1_ADIV(2) | /* ADIV=2:=40MHZ */
ADC_CFG1_MODE(1) | /* MODE=1: 12 bits ADC */
ADC_CFG1_ADICLK(0); /* ADICLK=0: use default pcc clock */

ADC0->SC1[0] = ADC_SC1_AIEN_MASK | /* AIEN=1: enable interrupt trigger */
ADC_SC1_ADCH(13); /* ADCH=13: use channel 13 */

ADC0->SC2 |= ADC_SC2_ADTRG(0); /* ADTRG=0: enable software trigger */
ADC0->SC3 = 0;

S32_NVIC->ICPR[ADC0_IRQn >> 5] = 1 << (ADC0_IRQn % 32); /* register ADC0 interrupt */
S32_NVIC->ISER[ADC0_IRQn >> 5] = 1 << (ADC0_IRQn % 32); /* enable ADC0 interrupt */
S32_NVIC->IP[ADC0_IRQn] = 0x0b;

adc_start_convert(13);

...
}

void
adc_start_convert(uint16_t adcChan)
{
ADC0->SC1[0] &= ~ADC_SC1_ADCH_MASK; /* Clear prior ADCH bits */
ADC0->SC1[0] = ADC_SC1_AIEN_MASK |
ADC_SC1_ADCH(adcChan);
}

void
ADC0_IRQHandler(void)
{
...
}

0 件の賞賛
返信
1 返信

1,726件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi

At the moment that you enabled the ADC interruption, you already have selected the channel. When ADC software trigger is configured, the conversion starts at the moment that the channel has been selected.

ADC0->SC1[0] = ADC_SC1_AIEN_MASK | /* AIEN=1: enable interrupt trigger */
ADC_SC1_ADCH(13); /* ADCH=13: use channel 13 */

ADC0->SC2 |= ADC_SC2_ADTRG(0); /* ADTRG=0: enable software trigger */‍‍‍‍

Best regards

Jorge Alcala

0 件の賞賛
返信