How to use ProcessorExpert set system clock to 80MHz?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use ProcessorExpert set system clock to 80MHz?

1,648件の閲覧回数
w_lingjun
Contributor III

Hi All,

I'm using S32K142 to develope, my S32DS version is "S32 Design Studio for ARM Version 2018.R1". And there is a  function named ProcessorExpert, it can config settings by GUI.

In the reference manual, normal RUN mode, the core and system clock can be set to 80MHz

But in the PE, it just can be set to 48MHz. So how to use PE set system clock to 80MHz?

1 返信

1,568件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Please refer to the following community post. 

Have a great day,

Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------