uja1169tk/f can not set partial networking

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uja1169tk/f can not set partial networking

ソリューションへジャンプ
1,461件の閲覧回数
jason_qian
Contributor I
I set CPNC = 1; when I read the register (0x22), the result is 0xc0, Please tell me which registers to set, thank you
0 件の賞賛
返信
1 解決策
1,451件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jason,

Please note that also the CWE bit should be set to 1:

7.8.JPG

The ID registers (0x27 to 0x2A) should also be configured so that UJA1169 knows which IDs are selected.

PNCOK bit should be set to 1 at the end of partial networking configuration:

Capture.JPG

I hope it helps.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,452件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jason,

Please note that also the CWE bit should be set to 1:

7.8.JPG

The ID registers (0x27 to 0x2A) should also be configured so that UJA1169 knows which IDs are selected.

PNCOK bit should be set to 1 at the end of partial networking configuration:

Capture.JPG

I hope it helps.

Best regards,

Tomas

0 件の賞賛
返信
1,440件の閲覧回数
jason_qian
Contributor I

jason_qian_0-1616030762949.png

jason_qian_1-1616030789498.png

jason_qian_2-1616031346846.pngjason_qian_3-1616031360830.pngjason_qian_4-1616031406856.png

 

I set the ID is 0x1a0,  Unable to wake up uja1169 when I send this ID once, but When I send it twice in a rowcan wake up  uja1169.   Why do I have to send the ID  twice in a row

0 件の賞賛
返信