uja1169tk/f can not set partial networking

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uja1169tk/f can not set partial networking

Jump to solution
1,454 Views
jason_qian
Contributor I
I set CPNC = 1; when I read the register (0x22), the result is 0xc0, Please tell me which registers to set, thank you
0 Kudos
Reply
1 Solution
1,444 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jason,

Please note that also the CWE bit should be set to 1:

7.8.JPG

The ID registers (0x27 to 0x2A) should also be configured so that UJA1169 knows which IDs are selected.

PNCOK bit should be set to 1 at the end of partial networking configuration:

Capture.JPG

I hope it helps.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
2 Replies
1,445 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jason,

Please note that also the CWE bit should be set to 1:

7.8.JPG

The ID registers (0x27 to 0x2A) should also be configured so that UJA1169 knows which IDs are selected.

PNCOK bit should be set to 1 at the end of partial networking configuration:

Capture.JPG

I hope it helps.

Best regards,

Tomas

0 Kudos
Reply
1,433 Views
jason_qian
Contributor I

jason_qian_0-1616030762949.png

jason_qian_1-1616030789498.png

jason_qian_2-1616031346846.pngjason_qian_3-1616031360830.pngjason_qian_4-1616031406856.png

 

I set the ID is 0x1a0,  Unable to wake up uja1169 when I send this ID once, but When I send it twice in a rowcan wake up  uja1169.   Why do I have to send the ID  twice in a row

0 Kudos
Reply