spi slave interrupt run off

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

spi slave interrupt run off

2,321 Views
zzqq
Contributor III

pastedImage_1.png

pastedImage_2.png

now bits/frame   is  80bits   (10bytes)

I can receive the 10 byte (0x99 0x88 0x77 0x66 0x55 0x44 0x33 0x22 0x11 0x00) sent to me by the main SPI
but I can receive onetime
0 Kudos
Reply
2 Replies

2,219 Views
zzqq
Contributor III
I can send the 10 byte (0x99 0x88 0x77 0x66 0x55 0x44 0x33 0x22 0x11 0x00) sent to me by the main SPI read
but I can receive onetime
0 Kudos
Reply

2,219 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Could you elaborate on the description or share a test code?

Do you see any SPI error flags? Does the SPI master transfer the data on the bus?

Regards,

Daniel

0 Kudos
Reply