show Ld error: undefined reference to and warning: cannot find entry symbol Reset_Handler;

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

show Ld error: undefined reference to and warning: cannot find entry symbol Reset_Handler;

6,489件の閲覧回数
jingfang
Contributor IV

 

I want MCAL Integrate Into S32 Design Studio,but:

show Ld error: undefined reference to and warning: cannot find entry symbol Reset_Handler; 

How can I slove it?

jingfang_0-1704272572680.png

jingfang_1-1704272577808.png

 

 

0 件の賞賛
返信
5 返答(返信)

6,464件の閲覧回数
NamLee
NXP Employee
NXP Employee

Hi jingfang,

I think your project is lacking resource files overall.

Please enter Properties and check all setup of compiler and linker resources.

Namm_0-1704363040262.png

One more point to check is the version of GCC, is that the version 10.2 is correct one which mentioned in Release Notes?

Thank you,

Nam.

 

0 件の賞賛
返信

6,463件の閲覧回数
NamLee
NXP Employee
NXP Employee

You can also refer to a project which can compiled done, for resource files/macros/links that it uses.

Thank you,

Nam.

0 件の賞賛
返信

6,426件の閲覧回数
jingfang
Contributor IV

LD I joined is 4.0.0.

jingfang_1-1704721146232.png

 

The project setting I copy "C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Adc_TS_T40D34M40I0R0\examples\S32DS\S32K3XX\Adc_example_S32K344\Project_Settings\Startup_Code" ,But there is still an error

jingfang_0-1704721037842.png

 

0 件の賞賛
返信

6,410件の閲覧回数
NamLee
NXP Employee
NXP Employee

Hi jingfang,

In the Project_Settings of project in workspace, inside the Linker_Files should have the .ld file like below:

Namm_0-1704770362846.png

The tool should automatically coppy the .ld file from C:\NXP\S32DS.3.5_2\S32DS\software\PlatformSDK_S32K3\RTD\Platform_TS_T40D34M30I0R0\build_files\gcc and link it in DS. Not manually coppy it.

Please help me to check again.

Is it possible if you can share your project here? You can export it and share the zip file here.

Namm_1-1704770601502.png

 

And you're using S32K RTD 4.0.0 is that correct? I want to check it directly for help you.

Thank you,

Nam.

0 件の賞賛
返信

6,408件の閲覧回数
NamLee
NXP Employee
NXP Employee

The S32DS\software\PlatformSDK_S32K3\RTD is the RTD package that you install in DS through updatesite one. It should be async with DS project for compiling and running tests.

Please help me to share your project.

Thank you,

Nam.

0 件の賞賛
返信