set flexcan to Listen-Only mode, RX interrupt abnormal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

set flexcan to Listen-Only mode, RX interrupt abnormal

3,548件の閲覧回数
liuning_neu
Contributor II

hi  nxp  S32K expert :

  

   I use S32K148,  for flexcan module,I want to Switch off transmit path, because i can not find the right way to do it, so i choose set flexcan  to  Listen-Only mode.  after i set  flexcan  to  Listen-Only mode, when flexcan receive a  can message, it enter  FLEXCAN_Error_IRQHandler,  not  enter FLEXCAN_IRQHandler.   my destination is  set  flexcan  to  Listen-Only mode,  when flexcan receive a  can message,  it enter FLEXCAN_IRQHandler.   in my opinion  ,the result  identify  RX interrupt are functional in LOM mode abnormally.

my question:

1:    I want to konw the result is right or wrong?  if it is wrong , what is the right way to realize it?

2:    Is there other way to realize  Switch off transmit path  of flexcan

my codes as following:

/* enter freeze mode */

 FLEXCAN_EnterFreezeMode(base);
/* Select mode */
FLEXCAN_SetOperationMode(base, FLEXCAN_LISTEN_ONLY_MODE);

/* exit freeze mode*/
FLEXCAN_ExitFreezeMode(base);

4 返答(返信)

3,465件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

it could be expected behavior, if a message is not acknowledged by other node

pastedImage_1.png

BR, Petr

0 件の賞賛
返信

3,465件の閲覧回数
liuning_neu
Contributor II

hi  Petr Stancik:

   how to realize  a message is acknowledged by other node?  could you tell me the specific operation or where i can get it ?

0 件の賞賛
返信

3,465件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you should have another active CAN node on the bus, which acknowledges the message. Every active node, that is able to transmit/receive, acknowledge a message on the bus, this is autonomous behavior as per CAN standard.

BR, Petr

3,465件の閲覧回数
liuning_neu
Contributor II

thank you very muchPetr Stancik

0 件の賞賛
返信