set flexcan to Listen-Only mode, RX interrupt abnormal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

set flexcan to Listen-Only mode, RX interrupt abnormal

3,552 Views
liuning_neu
Contributor II

hi  nxp  S32K expert :

  

   I use S32K148,  for flexcan module,I want to Switch off transmit path, because i can not find the right way to do it, so i choose set flexcan  to  Listen-Only mode.  after i set  flexcan  to  Listen-Only mode, when flexcan receive a  can message, it enter  FLEXCAN_Error_IRQHandler,  not  enter FLEXCAN_IRQHandler.   my destination is  set  flexcan  to  Listen-Only mode,  when flexcan receive a  can message,  it enter FLEXCAN_IRQHandler.   in my opinion  ,the result  identify  RX interrupt are functional in LOM mode abnormally.

my question:

1:    I want to konw the result is right or wrong?  if it is wrong , what is the right way to realize it?

2:    Is there other way to realize  Switch off transmit path  of flexcan

my codes as following:

/* enter freeze mode */

 FLEXCAN_EnterFreezeMode(base);
/* Select mode */
FLEXCAN_SetOperationMode(base, FLEXCAN_LISTEN_ONLY_MODE);

/* exit freeze mode*/
FLEXCAN_ExitFreezeMode(base);

4 Replies

3,469 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

it could be expected behavior, if a message is not acknowledged by other node

pastedImage_1.png

BR, Petr

0 Kudos
Reply

3,469 Views
liuning_neu
Contributor II

hi  Petr Stancik:

   how to realize  a message is acknowledged by other node?  could you tell me the specific operation or where i can get it ?

0 Kudos
Reply

3,469 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you should have another active CAN node on the bus, which acknowledges the message. Every active node, that is able to transmit/receive, acknowledge a message on the bus, this is autonomous behavior as per CAN standard.

BR, Petr

3,469 Views
liuning_neu
Contributor II

thank you very muchPetr Stancik

0 Kudos
Reply