s32k312 program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k312 program

Jump to solution
2,053 Views
lua40927
Contributor III

Hello

I am using S32K312EVB-Q172. The current PROJECT works normally in DEBUG mode.
My question is about burning. I used J-link to burn the bin file generated by the above project to the 0x400000 position. It showed that the burning was successful, but the program was not being executed.
I would like to ask if there are any steps or settings that are missing?

0 Kudos
Reply
1 Solution
2,006 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

This may caused by incorrect ratio between HSE_CLK and APIS_SLOW_CLK set by the Clocks Tool in S32CT. For more detail, please read the discussion in If I don't give s32k312 delay, the CAN stop during operation


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,007 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

This may caused by incorrect ratio between HSE_CLK and APIS_SLOW_CLK set by the Clocks Tool in S32CT. For more detail, please read the discussion in If I don't give s32k312 delay, the CAN stop during operation


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply