s32k3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k3

2,998 Views
hajianik
Senior Contributor I

Hi,

I installed DS 3.5 AND THE S32K3  DEVELOPMENT PACKAGE AND  3.5.0 RTM DRIVERS AND THERE IS NO EXAMPLE PROJECT ANYWHERE. WHERE WOULD I FIND SOME EXAMPLE PROJECTS?

for k3xx.

 

Thanks,

Koorosh Hajiani

Tags (1)
0 Kudos
Reply
4 Replies

2,961 Views
hajianik
Senior Contributor I

Hi Peter,

Thank you for your response.

I was able to get the examples. So I imported the project from this path:

C:\NXP\SW32K3_RTD_4.4_2.0.3\eclipse\plugins\Adc_TS_T40D34M20I3R0\examples\S32DS\Adc_example_S32K312,

how ever I can see the function definition and relevant header file are in in the folder one level higher than the example:

C:\NXP\SW32K3_RTD_4.4_2.0.3\eclipse\plugins\Adc_TS_T40D34M20I3R0\source  and

C:\NXP\SW32K3_RTD_4.4_2.0.3\eclipse\plugins\Adc_TS_T40D34M20I3R0\include

So my question is how to import this project so that the relevant files from the two folder shown above will be in the project.

 

Thanks,

Koorosh Hajiani

 

0 Kudos
Reply

2,910 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Looks like you will need to set the project paths for correct folders:

Here are the tutorials for S32DS:

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32DS-list-of-HOWTOs/ta-p/1113475

best regards,

Peter

0 Kudos
Reply

2,898 Views
hajianik
Senior Contributor I

Hi,

The link you sent is of absolutely no help. There is nothing on RTD, just SDK.

Anyways I'm closing this case.

 

Thanks,

0 Kudos
Reply

2,968 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Not sure about version RTD 3.5.0. but looking at recent available version 4.4.1 - the examples are inside plugins as usual.

petervlna_0-1689915835629.png

petervlna_1-1689915842854.png

Best regards,

Peter

0 Kudos
Reply