s32k3 update the source code error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k3 update the source code error

Jump to solution
1,593 Views
Alan_Y
Contributor II

Hello,

When I update the source code, the dialog box will show that the Clock and Peripheral have errors. I don't know why, because sometimes it works, sometime it have errors.

Thanks in advance!

Alan_Y_0-1674003639687.pngAlan_Y_0-1674003639687.png

 

Tags (2)
0 Kudos
Reply
1 Solution
1,583 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Alan,

According to the project name it looks like the project you imported is based on S32DS v3.4 + S32K3 RTD 0.9.0. Did you offline install this version of RTD?

Alan_Y_0-1674003639687.pngAlan_Y_0-1674003639687.png

You have not checked Clocks and Peripherals, please select them and switch to the Clocks and Peripheral interface to check for specific error messages.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,584 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Alan,

According to the project name it looks like the project you imported is based on S32DS v3.4 + S32K3 RTD 0.9.0. Did you offline install this version of RTD?

Alan_Y_0-1674003639687.pngAlan_Y_0-1674003639687.png

You have not checked Clocks and Peripherals, please select them and switch to the Clocks and Peripheral interface to check for specific error messages.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply