[s32k3] is it possible to re-flash unsecure software after secure boot enabled?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[s32k3] is it possible to re-flash unsecure software after secure boot enabled?

跳至解决方案
461 次查看
pasa_kevin_y
Contributor III

Once the hardware is in mass production stage, the secure boot is enabled, LC is OEM_PROD.

Say we found some issue in it, and we want to do some diagnostics.

We have the jtag access, we can re-flash another testing software to it, the entire flash memory will be overwritten, will the chip boot up with the unsecure software?  is NXP HSE allow it to happen?

0 项奖励
回复
1 解答
398 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @pasa_kevin_y 

When you flash a new application to the device, there is the specific bit in the IVT (Image Vector Table) that controls whether Secure Boot is enabled. If you remove the Secure Boot bit in the IVT, the device will not perform a secure boot.  This means the boot process will skip the security checks that normally verify the integrity and authenticity of the application.

 

BR, VaneB

在原帖中查看解决方案

1 回复
399 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @pasa_kevin_y 

When you flash a new application to the device, there is the specific bit in the IVT (Image Vector Table) that controls whether Secure Boot is enabled. If you remove the Secure Boot bit in the IVT, the device will not perform a secure boot.  This means the boot process will skip the security checks that normally verify the integrity and authenticity of the application.

 

BR, VaneB