s32k14x PLL Frequency Tolerance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s32k14x PLL Frequency Tolerance

跳至解决方案
5,451 次查看
Mimo88
Contributor I

I'm trying to figure out the S32k14x PLL frequency tolerance, I found in the data sheet the following table that specify the lock exit frequency tolerance Dunl value. I'm a little bit confused if this value represent the PLL frequency tolerance. if no where i can find this info?

Mimo88_0-1602774194085.pngMimo88_0-1602774194085.png

 

0 项奖励
回复
1 解答
5,439 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

The table specifies typ. PLL Jitter over one PLL period and accumulated jitter over 1us.

 

BR, Daniel

在原帖中查看解决方案

0 项奖励
回复
4 回复数
5,142 次查看
aceangle
Contributor II

it seems the accuracy is kind of high. say  Fvco_clk =320M, the period is 3.125ns, so the tolerance is 75ps/3.125ns=2.4%.

but I do not know whether the calculation method is right or not.  maybe there exists other calculation method I do not know.

do you have any ideas?

0 项奖励
回复
5,440 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

The table specifies typ. PLL Jitter over one PLL period and accumulated jitter over 1us.

 

BR, Daniel

0 项奖励
回复
5,142 次查看
aceangle
Contributor II

Hi, Daniel

Could you please show how to calculate the accuracy of PLL? let's say Fvco_clk=320MHz. could you show the detailed calculation?

is the calculation right or not: 75ps/(1000/320ns)=2.4% ?

I also have to calculate UART baudrate(20kbps) accuracy, which is derived from SPLL_CLK.

aceangle_1-1636083869631.pngaceangle_1-1636083869631.png

aceangle_0-1636084000145.pngaceangle_0-1636084000145.png

 

 

 

标记 (1)
0 项奖励
回复
5,363 次查看
gobrien8
Contributor I

Daniel, 

I have the same question about the PLL Lock Exit Frequency Tolerance.  If we are trying to quantify the overall PLL timing error say over a 1uS period, is the long term jitter all that we consider?  Does the PLL Lock Exit Frequency Tolerance have any bearing on the timing error in this case? 

0 项奖励
回复