- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
i use can for bootloader and use expert to generate the can driver.
set boot ld
/* Specify the memory areas */
MEMORY
{
/* Flash */
m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000400
m_flash_config (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010
m_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x0001fbf0 /*0x0017FB00*/
/*m_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x0017FB00*/
/*m_flash_app_head (RX) : ORIGIN = 0x0017FF10, LENGTH = 0x000000F0*/
/* SRAM_L */
m_data (RW) : ORIGIN = 0x1FFE0000, LENGTH = 0x00020000
/* SRAM_U */
m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x0001EFF8
/* Reserved 64K data flash for EEPROM emulator (m_flexram) */
m_flexram (RW) : ORIGIN = 0x14000000, LENGTH = 4K
}
app ld file
m_interrupts (RX) : ORIGIN = 0x00020000, LENGTH = 0x00000400
m_flash_config (RX) : ORIGIN = 0x00020400, LENGTH = 0x00000010
m_text (RX) : ORIGIN = 0x00020410, LENGTH = 0x0015FB00
use JumpToUserApplication();
the go to 0x20000 run app that work passed.
but the interrupt can't work at app side.
the all isr can't work and lock at OSIF_SemaWait();
because the isr SysTick_Handler() not work.
attached zip file
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Have you relocated the vector table address before the jump?
S32_SCB->VTOR = (uint32_t)APP_START_ADDRESS;
However, I have found a similar thread where is solved a similar issue:
https://community.nxp.com/t5/S32K/Interrupt-can-t-work-in-application/m-p/674635
Best regards,
Diana
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Have you relocated the vector table address before the jump?
S32_SCB->VTOR = (uint32_t)APP_START_ADDRESS;
However, I have found a similar thread where is solved a similar issue:
https://community.nxp.com/t5/S32K/Interrupt-can-t-work-in-application/m-p/674635
Best regards,
Diana
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
if i use debug tools go to Reset_Handler() that isr can't work.
it's go to address 0x0000908
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
yes ! INT_SYS_DisableIRQGlobal();
JumpToUserApplication(*((uint32_t*)APP_START_ADDRESS), *((uint32_t*)(APP_START_ADDRESS + 4)));
APP_START_ADDRESS 0x20000
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I have made some tests with the serial bootloader and application which uses SysTick interrupt.
After adding "S32_SCB->VTOR = (uint32_t)APP_START_ADDRESS ;" into application project the interrupt starts working.
After the jump into the application project the VTOR register is reset, so, the vector table needs to be relocated directly in the application project.
I believe it helps.
Best regards,
Diana
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
which c file add the "S32_SCB->VTOR = (uint32_t)APP_START_ADDRESS ;"?
void init_data_bss(void) of startup.c.
i don't know which file add "S32_SCB->VTOR = (uint32_t)APP_START_ADDRESS ;" was right.
please tell me.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I'm sorry, I have used it in main.c.
Best regards,
Diana
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
i resolve the app can't interrupt.
bootloader side :
canflash finishing don't use JumpToUserApplication(...); to app.
because the bootloader i have use isr for can,ptc,time isr. if use JumpToUserApplication() that isr irq may trigger,
than at app the __VECTOR_TABLE incorrect trigger.
1.canflash finishinh so needs use than set flag to ram PAddress=0x55aaaa55;
2.SystemSoftwareReset();
3.the bootloader sw reset than check PAddress=0x55aaaa55;
4.go to JumpToUserApplication()
app to bootloader don't use JumpToUserApplication()
1.stop all isr,set ram/rom flag
2.use SystemSoftwareReset(); than go to bootloader
3.bootloader check the ram/rom flag ;if set goto canflash.
i think the was startup_S32K148.s bug .
because the Reset_Handler just disable INT_SYS_DisableIRQGlobal();,but isr trigger true exist at boot or app.
so the boot to app DisableIRQGlobal only disable Global isr ,bit unit isr true work.
to go app the isr trigger at app side,than app relocal __flash_vector_table__ can't correct trigger at app isr.
but detail may nxp can try it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
add S32_SCB->VTOR= (uint32_t)0x20000; at main
I TRY the interrupt can't work.
please tell me how to debug the Global interrupt address.
the ptc isr can't work.