s32k144 pwm issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k144 pwm issue

3,317件の閲覧回数
alice_th
Contributor III

Hello,

when use FTM PWM, i find when use uart to printf the log, the PWM doesn't work,

but when remove printf, then the pwm output the correct waveform.

could you help to check it what is the reason ? 

i attached the project, please test it.

void test_pwm()
{
    //pwm_init();
    uint16_t duty_cycle[] = {0,0x2000,0x4000,0x6000,0x8000};
    uint8_t len = sizeof(duty_cycle)/sizeof(uint16_t);
    status_t st = STATUS_SUCCESS;
    while(1)
    {
        for(uint8_t i = 0;i<len;i++)
        {

            //set_pwm_duty_cycle(0,duty_cycle[i]);
            st = FTM_DRV_UpdatePwmChannel(INST_FLEXTIMER_PWM_1,
                                                 flexTimer_pwm_1_IndependentChannelsConfig[0].hwChannelId,
                                                 FTM_PWM_UPDATE_IN_DUTY_CYCLE, duty_cycle[i],
                                                 0U,
                                                 true);
            printf("duty_cycle=0x%x,pwm status=0x%x\n\r",duty_cycle[i],st);
            OSIF_TimeDelay(100);
            //OSIF_TimeDelay(10000);
        }

    }
}
see the log, when add these printf, pwm status return 1 = STATUS_ERROR

duty_cycle=0x0,pwm status=0x1
duty_cycle=0x2000,pwm status=0x1
duty_cycle=0x4000,pwm status=0x1
duty_cycle=0x6000,pwm status=0x1
duty_cycle=0x8000,pwm status=0x1

タグ(1)
0 件の賞賛
返信
14 返答(返信)

3,189件の閲覧回数
alice_th
Contributor III

here is the new project, please help to check it, thank you! @danielmartynek 

0 件の賞賛
返信

3,272件の閲覧回数
alice_th
Contributor III

can anybody who help test and answer this question, thank you very much! 

0 件の賞賛
返信

3,257件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Alice,

There is something wrong with the console lib, but we don't have the capacity to debug this SW.

Why don't you use the LPUART SDK driver directly?

The printf() uses LPUART_1 anyway.

 

Regards,

Daniel

 

0 件の賞賛
返信

3,220件の閲覧回数
alice_th
Contributor III

do you have examples about printf ?

if use directly LPUART SDK driver, there some transfer when need print different variable

0 件の賞賛
返信

3,215件の閲覧回数
alice_th
Contributor III

@danielmartynek i try it with this

 

void uart_printf(const char *ptr)
{
uint32_t bytesRemain;
size_t bytes=strlen(ptr);
// unsigned char ret_car[]={"\r"};
LPUART_DRV_SendData(INST_LPUART_1, (uint8_t *)ptr, bytes);
while(LPUART_DRV_GetTransmitStatus(INST_LPUART_1, &bytesRemain) != STATUS_SUCCESS);
// LPUART_DRV_SendData(INST_LPUART1, ret_car, 1);
// while(LPUART_DRV_GetTransmitStatus(INST_LPUART1, &bytesRemain) != STATUS_SUCCESS);
}

void test_pwm()
{
//pwm_init();
uint16_t duty_cycle[] = {0,0x2000,0x4000,0x6000,0x8000};
uint8_t len = sizeof(duty_cycle)/sizeof(uint16_t);
status_t st = STATUS_SUCCESS;
while(1)
{
for(uint8_t i = 0;i<len;i++)
{
 
//set_pwm_duty_cycle(0,duty_cycle[i]);
st = FTM_DRV_UpdatePwmChannel(INST_FLEXTIMER_PWM_1,
                                     flexTimer_pwm_1_IndependentChannelsConfig[0].hwChannelId,
FTM_PWM_UPDATE_IN_DUTY_CYCLE, duty_cycle[i],
                                     0U,
                                     true);
uart_printf("test_pwm\n\r");
OSIF_TimeDelay(100);
//OSIF_TimeDelay(10000);
}
 
}
}
still the same, there is no pwm output when use uart_printf, could you help to check, how to implement the printf funciton , thank you very much!

 

0 件の賞賛
返信

3,201件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @alice_th,

Can you send the new project?

 

Thank you

0 件の賞賛
返信

3,111件の閲覧回数
alice_th
Contributor III

@danielmartynek any feedback , thanks!

0 件の賞賛
返信

3,074件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @alice_th,

Sorry for the delay, I could not get to the testing because of the overload.

Can you declare ftm_state_t ftmStateStruct as a global variable?

0 件の賞賛
返信

3,014件の閲覧回数
alice_th
Contributor III

after set ftm_state_t ftmStateStruct as a global variable, now it works even with printf(the console lib) it still can work, why need set as a global variable ?

0 件の賞賛
返信

3,007件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @alice_th,

I'm glad it works now.

Because you are calling the APIs of the driver from different functions that must access the struct.

 

 

 

 

0 件の賞賛
返信

2,994件の閲覧回数
alice_th
Contributor III

hello @danielmartynek 

when i set with dead time, ch1 don't have waveform output, could you help to check it 

 

alice_thanks_0-1728530394416.png

alice_thanks_1-1728530478492.png

look at ch1 with green line, no pwm output

alice_thanks_2-1728530685331.pngalice_thanks_3-1728530714604.png

 

0 件の賞賛
返信

2,971件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @alice_th,

This is not related to the topic of this thread.

Please create a new one.

 

Thank you

0 件の賞賛
返信

2,992件の閲覧回数
alice_th
Contributor III

here is attached

0 件の賞賛
返信

3,161件の閲覧回数
alice_th
Contributor III

here is the project @danielmartynek 

0 件の賞賛
返信