s32k144 csec secure boot BOOT_MAC update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k144 csec secure boot BOOT_MAC update

Jump to solution
2,933 Views
kmh48301
Contributor IV

Hi

How can I update BOOT_MAC when secure boot is activated.

!!! I need to avoid erasing csec keys (returning to factory state). !!!

 

Thanks

Best Regards

Phillip

0 Kudos
Reply
1 Solution
2,924 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Phillip,

this is described in the AN5401:

lukaszadrapa_0-1628667777442.png

 

So, the procedure is the same as when updating a key. You just need to calculate the new BOOT_MAC somehow.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
2 Replies
2,925 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Phillip,

this is described in the AN5401:

lukaszadrapa_0-1628667777442.png

 

So, the procedure is the same as when updating a key. You just need to calculate the new BOOT_MAC somehow.

Regards,

Lukas

0 Kudos
Reply
2,568 Views
cychen88
Contributor II

if Secure Boot Modes is Strict Sequential Boot Mode,when secure boot check is error the flash system comes out of RESET,How to recover in this case?

0 Kudos
Reply