s32k144 csec secure boot BOOT_MAC update

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k144 csec secure boot BOOT_MAC update

ソリューションへジャンプ
2,890件の閲覧回数
kmh48301
Contributor IV

Hi

How can I update BOOT_MAC when secure boot is activated.

!!! I need to avoid erasing csec keys (returning to factory state). !!!

 

Thanks

Best Regards

Phillip

0 件の賞賛
返信
1 解決策
2,881件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Phillip,

this is described in the AN5401:

lukaszadrapa_0-1628667777442.png

 

So, the procedure is the same as when updating a key. You just need to calculate the new BOOT_MAC somehow.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,882件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Phillip,

this is described in the AN5401:

lukaszadrapa_0-1628667777442.png

 

So, the procedure is the same as when updating a key. You just need to calculate the new BOOT_MAC somehow.

Regards,

Lukas

0 件の賞賛
返信
2,525件の閲覧回数
cychen88
Contributor II

if Secure Boot Modes is Strict Sequential Boot Mode,when secure boot check is error the flash system comes out of RESET,How to recover in this case?

0 件の賞賛
返信