s32k144 FTM_SignalMeasurement_Example can not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k144 FTM_SignalMeasurement_Example can not work

1,792件の閲覧回数
jiangbolwj
Contributor II

QQ截图20170711165122.png

i use the example to  test but can not work ,i did not connect error the line ,two line is pTC0 and PTB2,

when I test I find it could not into the interrupt,I change the PORT of the INPUT ,it can not work

it have PWM out ,but the input part can not work,

what is the problem, i am crazy,could you help me

0 件の賞賛
返信
1 返信

1,631件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

same as this thread https://community.nxp.com/thread/455092 

See discussion there...

BR, Petr

0 件の賞賛
返信