s32k144 FLEXCAN TXD, RXD Impedance content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k144 FLEXCAN TXD, RXD Impedance content

Jump to solution
2,069 Views
jung_ho_lee
Contributor I

Chipset: S32K144HAT0VLH
Function: FLEXCAN
               TXD (PTC3)
               RXD (PTC2)
Implementation:

                           Implementation of communication without using CAN transceiver.

Question:

                 Is there a method or manual to check the impedance of TXD and RXD pins?

 

Thanks.

0 Kudos
Reply
1 Solution
2,028 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

TXD (PTC3) / RXD (PTC2) are normal IO pins so refer to datasheet for I/O parameters.

If you want to connect nodes without transceiver on short distance on PCB below connection is commonly used

 

PetrS_1-1652774944273.png

BR, Petr

View solution in original post

0 Kudos
Reply
1 Reply
2,029 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

TXD (PTC3) / RXD (PTC2) are normal IO pins so refer to datasheet for I/O parameters.

If you want to connect nodes without transceiver on short distance on PCB below connection is commonly used

 

PetrS_1-1652774944273.png

BR, Petr

0 Kudos
Reply