please help me about sdk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

please help me about sdk

Jump to solution
1,302 Views
ssslz
Contributor III

When I create a new project, I select the SDK as PlatformSDK_S32K3_2022_03_S32K344_M7, but the generated mex file has the SDK as PlatformSDK_S32K3_2022_07_S32K344_M7. What method can I use to make both SDKs become either PlatformSDK_S32K3_2022_03_S32K344_M7 or PlatformSDK_S32K3_2022_07_S32K344_M7?

1111.png222.png

0 Kudos
Reply
1 Solution
992 Views
ssslz
Contributor III
0 Kudos
Reply
4 Replies
1,270 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ssslz 

First, please note that RTD versions 2.0.0 and 2.0.1 are older software releases, and we recommend updating to newer IDE and RTD versions.

Regarding your question about converting or aligning both SDKs to either PlatformSDK_S32K3_2022_03_S32K344_M7 or PlatformSDK_S32K3_2022_07_S32K344_M7, this is not possible. The two versions cannot be merged or converted into a single SDK. You must choose and work with either RTD version 2.0.0 or RTD version 2.0.1, depending on your project requirements.

Finally, with the latest releases of S32 Design Studio, it is recommended to install only one RTD version per device to ensure correct functionality and avoid conflicts within the IDE.

 

BR, VaneB

0 Kudos
Reply
1,053 Views
ssslz
Contributor III
What I mean is, why is the SDK I selected in the project PlatformSDK_S32K3_2022_03_S32K344_M7, but the SDK in the generated MEX file is PlatformSDK_S32K3_2022_07_S32K344_M7? What I mean is, how can I make both the SDK in the project and the SDK in the MEX file become PlatformSDK_S32K3_2022_03_S32K344_M7, instead of merging these two SDKs into one.
0 Kudos
Reply
1,021 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ssslz 

This behavior is typically caused when multiple RTD versions for the same device family are installed within a single S32DS instance. As a best practice, it is recommended to have only the specific RTD version you intend to use installed.

Please try uninstalling all existing RTD versions, and then install only the required version. This should help resolve the issue.

0 Kudos
Reply
993 Views
ssslz
Contributor III

thank you

0 Kudos
Reply